Drive_Working_Settings_Extended
Drive_Working_Settings_Extended
| Address: | 8707 (2203H) | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Type: | WORD | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Access: | Read/Write | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Unit: | -- | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Range: | 0 to 65535 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Default Value: | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Store Supported: | Yes | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Description: |
This register is used to parametrize drive working modalities.
Bit Explanation:
Disable_Fault_Output: When this bit is set (1) the B0_Out0 digital output is free for the user application. When this bit is reset (0) the B0_Out0 is automatically handled by the drive's firmware as Fault Output.
Disable_Auto_Motor_Enable: When this bit is set (1) the motor will remain disabled at switch on (Master_Register bit #0 = 0). When this bit is reset (0) the motor will be automatically enabled at switch on (Master_Register bit #0 = 1).
EncoderX_Rotation_Direction: When this bit is set (1) the Encoder #X counting is reversed. When this bit is reset (0) the Encoder #X counting is not reversed.
RL_Motor_Detection: When this bit is set (1) the Motor Parameters (Resistance and Inductance) are detected automatically at switch-on (Nominal_Current object need to be set). When this bit is reset (0) the Motor Parameters (Resistance and inductance) are not detected automatically and must be set on objects Motor_R and Motor_L.
Motor_Stall_detection (1): When this bit is set (1) the ‘Motor Stall detection’ feature is enabled. When this bit is reset (0) the ‘Motor Stall detection’ feature is disabled.
The ‘Feedack’ feature (bit 4 of Drive_Working_Settings object) and ‘Motor Stall detection’ feature (bit 13 of Drive_Working_Settings_Extended object) cannot be both active at the same time otherwise an alarm is issued (bit 5 of Error_Register object and bit 14 of Feedback_Status) . |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Notes: | (1) The ‘Motor Stall detection’ feature is available only with firmware version V02r74 or superior. |